Skip to main content
Visitor II
May 18, 2005
Question

programmer problem

  • May 18, 2005
  • 2 replies
  • 652 views
Posted on May 18, 2005 at 08:36

programmer problem

    This topic has been closed for replies.

    2 replies

    huaer2000Author
    Visitor II
    May 9, 2005
    Posted on May 09, 2005 at 12:51

    dear sjo,

    I have made flashbash and successful to program st72c334n4.

    now i use it to program st7flite09 and found some problem. programmer serial port test is ok, I can write optionbyte, but I

    can not write the flash erea. an error message is displayed

    ''operation Failed'' , coudl you help me solve this problem.

    best regards,

    Visitor II
    May 18, 2005
    Posted on May 18, 2005 at 08:36

    If option bytes are being programmed successfully, it indicates successful communication and proper Flash function/ICC. But, did you check the Flash memory mapping in the 334 you are using and the Lite09?