I am at my wits end trying to make my code work. I have a uPSD3333DV on a designed board, but am also trying the code on a DK3300-ELCD. I am writing C with RIDE. I am able to JTAG both. I have simplifed my code to the following:
void main(void) { RCAP2H = 0xFF;//Sets baud rate at 115200 RCAP2L = 0xF5;//for both UART0 and UART1 T2CON = 0x34; // sets timer 2 for both R/T baud rates SCON0 = 0x74; while(1) { SBUF0 = 'H'; msDelay(10); } } I have a subroutine for the msDelay function, but cannot even get either processor to send out a ''Hello World'' from the serial port... The CAPs and PSDsofware Express are extremely confusing... I would imagine my code is so basic that this must be a CAP configuration issue... HELP!!!
P3SFS = 0x03;//Enable UART on Port 3 PS0 = 0;//Set UART0 for Priority status PCON |= 0x80; This at least made the serial port do something (an endless string of '6's).
So making thoses changes at least made all the code work in the RIDE simulator. One odd thing... in the RIDE simulator UART1 is showing up for BAUD and everything for Timer 1 instead of Timer 2. It was my desire to use Timer 2 to generate the transmit and receive Baud rate for both UART0 and UART1. Anyone know how to configure this?
Gosh... feel like I am talking to myself alot - anyone reading these?
I'm trying to get familiar with thy upsd 3334. On my way I succeed programming the uarts with differnt baudrates, by using the keil compiler. When you need two differnt baudrates, it is necessary to use timer 2 for uart 0 and timer 1 for uart 1. I know that it is possible to use one timer if you want one baudrate for both uarts, but i've never test this possibility. Perhaps you can find a solution for your problem in my source. regards Horst