Skip to main content
Visitor II
August 4, 2004
Question

PSD logic problens

  • August 4, 2004
  • 1 reply
  • 576 views
Posted on August 04, 2004 at 18:25

PSD logic problens

    This topic has been closed for replies.

    1 reply

    sbencke3Author
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:02

    Hi,

    I’m having some problems with my project somebody can help me?

    My memory map is:

    Main Flash:

    FS0 – PAG: 0 – 0X0000 ~ 0X3FFF

    FS1 – PAG: 0 – 0X4000 ~ 0X7FFF

    FS2 – PAG: 0 – 0X8000 ~ 0XBFFF

    FS3 – PAG: 0 – 0XC000 ~ 0XFFFF

    Others:

    RS0 – 0XC000 ~ 0XDFF

    CSIOP – 0XE00 ~ 0XE0FF

    LCD_E – 0XE100 ~ 0XE1FF

    Secondary flash:

    CSBOOT0 – 0X0000 ~ 0X1FFF

    CSBOOT1 – 0X2000 ~ 0X3FFF

    CSBOOT2 – 0X4000 ~ 0X5FFF

    CSBOOT3 – 0X6000 ~ 0X7FFF

    Main Flash: Data Space Only

    Secondary Flash: Program Space Only

    I’m running my IAP application at CSBOOT flash, but I can’t make my LCD routines works. If I put this same program at the main flash it works fine. Can it happen because my LCD_E logic is mapped in the same address of main flash? How can I resolve this?

    Thanks in advance

    Sombra