Skip to main content
Visitor II
December 27, 2009
Question

PSRAM Interfacing

  • December 27, 2009
  • 3 replies
  • 720 views
Posted on December 27, 2009 at 19:23

PSRAM Interfacing

    This topic has been closed for replies.

    3 replies

    mmgbmmAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 10:00

    Hi,

    I’m trying to interface STR911FAW44X6 to a PSRAM device (MT45W4MW16BCGB). Unfortunately we’re using the LQFP128 package, which means we have to use some extra logic to get the correct interface.

    The problem I have at the moment is that EMI_WRHn and EMI_WRLn are pulled low during a read cycle! Is there a register I have to set to prevent this?

    We’re using Asynchronous mode only. The decode logic is:

    UBn = EMI_WRHn & EMI_RDn

    LBn = EMI_WRLn & EMI_RDn

    WEn = EMI_WRHn & EMI_WRLn

    Any help would be appreciated.

    Thanks,

    MM

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 10:00

    Hi mmgbmm

    Strange behavior!!!!

    Could you please confirm that the default state of both EMI_WRHn & EMI_WRLn just after Reset is high ?

    Normally all EMI control signal are output high state after and during RESET.

    Cheers.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 10:00

    Looks to me like misconfiguration of SCU_EMI register (LFBGA/LQFP), kinda like WRh/WRl work like UB/LB.

    Try to change (see the register description in RM).