I need to have some variables that retain their values when the CPU is reset or powered off. I'm using the IAR dev. system, and the only way I can see to do it is by using their ''@'' and ''__no_init'' C extensions that allow you to specify an actual memory location for a variable and leave it uninitialized by the compiler. So I tried the following code:
__no_init char NonVolatile[40] @ 0x20000; .... NonVolatile[0] = 'A'; putchar(NonVolatile[0]); I have tried a lot of different memory addresses beside 0x20000, with the same results -- the contents of NonVolatile[0] is always a blank (32). Can anyone tell me how to do this properly?