Question on Gate driver (L6491) on the STEVAL-CTM009V1 board
Hi Sir/Ma'am,
I have a question about the gate driver L6491 on the STEVAL-CTM009V1 board
Explanation: Currently, I am using the STEVAL-CTM009V1 evaluation kit for my motor control application. I have connected the necessary power supplies(48V and 12V) and all 4 RED LEDs are ON. I applied 6 PWMs and tested that I could see the PWMs at the input of the gate driver. but I am not receiving any output other than small spikes at the low sides output and LOW at high sides output..
Questions: what could be the reason behind this? As per my understanding, Is it a problem with the SD/OD pin?(see figure below from datasheet) Do I need to apply High input to this pin? if yes, how? And how much? Is it 3.3 V or 5 V? Or the problem is something else?

Please also let me know if I need to take care of any other things while working with this board.
Best regards,
Nayan