Skip to main content
Visitor II
June 4, 2020
Question

Question regarding the Programmer(Jtag) for ST10F276E supported

  • June 4, 2020
  • 1 reply
  • 1140 views

Hi Team,

I am working with ST10F276E Micro controller being MDK-arm not supported installed C166 toolchain eveluation version and it was successfully build.

My question that i want to download the code into flash (microchip IC) i found something like 

JTAGjet-166(http://www.keil.com/dd/chip/3545.htm)its with IAR embedded workbench.

So, is there any flash utility to support downloading the hex file into the flash using UART calble or any ST-link/u-link debugger(JTAG) to purchase..???

Kindly suggest.. :)

    This topic has been closed for replies.

    1 reply

    Graduate II
    June 4, 2020

    Like ST10 Flasher?​

    MNageAuthor
    Visitor II
    June 4, 2020

    hope u got my question i mean to say do i no need to use any STlink debugger (adapter) as interface to pc and board (if need to use i dont have connection setup at boradside) so directly thrpugh UART interface can ST10 flasher will work...????

    Graduate II
    June 4, 2020

    You're using an obsolete device. What active support there used to be has moved on.

    I'm answering the question : "So, is there any flash utility to support downloading the hex file into the flash using UART cable"

    Yes, there's a tool called ST10 Flasher that does exactly that.

    https://www.st.com/resource/en/application_note/cd00052666-programming-the-st10f27x-embedded-flash-using-the-st10flasher-tool-stmicroelectronics.pdf

    Not sure how well it handles COM ports with high indicies, really OLD software.

    https://community.st.com/s/question/0D53W000004lNH9SAM/how-can-i-get-the-st10-flasher-tool