Skip to main content
Visitor II
September 10, 2004
Question

re program failed since after first 2 to 3 times programming OK!

  • September 10, 2004
  • 5 replies
  • 802 views
Posted on September 10, 2004 at 06:00

re program failed since after first 2 to 3 times programming OK!

    This topic has been closed for replies.

    5 replies

    hg-chenAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:02

    uPSD3234BV-24U6 is used.

    at first 2 to 3 times, programing is OK, but since then,

    re program failed!

    any suggestion?
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:02

    Verify that the FlashLink device and JTAG connection to the DK3200 is good by running the FlashLink Connect Test and the Target Connect Test (these tests are found in the H/W setup located in the JTAP-ISP Operations Window). Be sure to do an erase all in case the security bits were set. Check your power supplies to the device.

    hg-chenAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:02

    Error message as below: also attachement

    Erse Full chip----Fail

    Fail to erase full chip

    Program operation unsuccesul----
    hg-chenAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:02

    error message as attachement

    hg-chenAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:02

    the loop test result as attachement!

    any idea?