Regarding Flash Size and Revision ID of the MicroController stm32F4
I Having Two Board In which stm32F439nI Micro-Controller Mounted on it. While Connecting with the STM Utility Software , one Board Display flash Size but didn't Show revision Id, Same Way i Connected Another board but it Doesn't Display Flash Size neither Revision Id.
In 1st Board am Available to Flash Directly Using the IJET Debugger but in 2nd Board I have to Flash Code with Help of STM ultility Software.
I Checked the Firmware Version Both Having Same but in Option Byte option only one Difference, in Working Board DB1M Option Unchecked While in Another Non Working Board DB1M is Checked.
Am Also Attaching the Working and Non Working Board STM Utlility Software