Skip to main content
Visitor II
January 7, 2004
Question

reset by JTAG

  • January 7, 2004
  • 2 replies
  • 685 views
Posted on January 07, 2004 at 18:21

reset by JTAG

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:57

    hello,

    We are trying to implement the hardware watchdog with uPSD3233B. According to my knowledge,flash link (JTAG)cable pin8 is connected to reset pin of uPSD.

    During ISP,whether the naual reset will affect the JTAG operation of programming or not??

    hat i have observed is,during ISP using JTAG,all the port lines of uPSd are in input state (logic 1).,so in this state , hardware atchdog refreshing is no longer possible.If we conside the watchdog time out to be second, controller should get reset in between the programming.

    but it's not the case.

    i would like to know the reason behind the same.

    Regards,

    Purvi

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:57

    During JTAG ISP operation, the Reset on the JTAG IP is holding off the the Reset from the MCU side, therefore the MCU Watchdog function is not working during PSD (flash memory) access time.