Skip to main content
Visitor II
October 6, 2005
Question

Reset capacitance to allow ICP

  • October 6, 2005
  • 2 replies
  • 819 views
Posted on October 06, 2005 at 19:11

Reset capacitance to allow ICP

    This topic has been closed for replies.

    2 replies

    dave5Author
    Visitor II
    July 21, 2005
    Posted on July 21, 2005 at 14:12

    I cannot get the Scotty board to in-circuit program an ST7flite0 device, when a 100nF capacitor is attached to the reset pin. Is their a maximum capacitance that can be used? Why does the evaluation board supplied with Scotty not have a capacitor at all on the reset pin?

    Visitor II
    October 6, 2005
    Posted on October 06, 2005 at 19:11

    Hopefuly you have already found a solution, but I experienced the same problems. Unforunately the Scotty guide states a minimum pull-up resistor value of 1K but states nothing about the reset capacitor. I have been informed the evaluation board is reset using the low voltage detector.