Skip to main content
Visitor II
November 24, 2003
Question

reset the timers

  • November 24, 2003
  • 5 replies
  • 1322 views
Posted on November 24, 2003 at 13:51

reset the timers

    This topic has been closed for replies.

    5 replies

    adi2Author
    Visitor II
    November 24, 2003
    Posted on November 24, 2003 at 12:01

    hi !

    when i use the output compare function , when i'm writing to the CLR register will it reset the counter ????

    thanks.

    adi
    Visitor II
    November 24, 2003
    Posted on November 24, 2003 at 12:08

    Which device are you using??

    adi2Author
    Visitor II
    November 24, 2003
    Posted on November 24, 2003 at 12:17

    st72264

    Visitor II
    November 24, 2003
    Posted on November 24, 2003 at 12:56

    Yes, while using 16-bit timer/output compare function , the counter is reset by writing into the count low register(CLR). It is also mentioned into the datasheet.

    adi2Author
    Visitor II
    November 24, 2003
    Posted on November 24, 2003 at 13:51

    yes ,it is written in the datasheet but not under the output compare function section and i just wanted to be sure.

    thanks.