Skip to main content
Visitor II
April 6, 2006
Question

RLINK - FLINK

  • April 6, 2006
  • 2 replies
  • 814 views
Posted on April 06, 2006 at 19:04

RLINK - FLINK

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:07

    Ciao,

    I have problems in using the RLINK to program a uPSD3233B on board.

    I'm able to erase , execute a blank test, and on a programmed part execute the verify, but when I try to program it I always get the following error:

    PSDsoft Express 8.30 Copyright (C) 1993-2004 STMicroelectronics, Inc. All Rights Reserved.

    DATE : 06/15/2005 TIME : 12:22:24

    Device 1 : ( 4 pins )

    Program ...

    Erasing ...

    Programming/Verifying...

    fail

    Program/verify operation unsuccessful ...

    ERROR: Data (0600)

    Hint: Programming failure.

    Time elapsed : 6 sec.

    By the way, if I use the Flashlink on the same board, I've no problems.

    I also changed the Rlink, assuming it was damaged, but no changes.

    Any idea?

    Thanks

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:07

    I am getting this same problem. I can't explain why. The osf file is created correctly. I am using a PSD4256G6V.