RTC Issue
We have a Load-Rite Pro LR918 loader scale. The device does not keep time anymore.You can set the time but it doesn't advance at a proper rate and usually within 1 week it is about 6 days behind. I opened up the scale main control unit hoping to find a battery but there was none there. I looked into it further and found a M48T35Y-70PCI RTC module in there. We have had this scale for about 5-7 years now if not longer plus the loader at times sits for days on end without being used so I am assuming whatever battery is keeping the time is dead or almost dead as this is something that has only become an issue within the last couple weeks as it seemed to have been working good up till then. Is this device replaceable or is the battery inside it replacable? I have found a complete replacement device on the digikey website but after doing some reading it looks like it needs to be programmed before using if I am not mistaken and if that is the case I have no way to program it so I would prefer to do a internal battery replacement if possible. Also, is there any way to do some self diagnosing on this device to know for sure if it is a battery issue or not.
Your help would be greatly appreciated.