Skip to main content
Visitor II
May 20, 2004
Question

Sector 0 in FLASH program memory (ST7LITE2)

  • May 20, 2004
  • 2 replies
  • 851 views
Posted on May 20, 2004 at 11:46

Sector 0 in FLASH program memory (ST7LITE2)

    This topic has been closed for replies.

    2 replies

    hkurtAuthor
    Visitor II
    May 18, 2004
    Posted on May 18, 2004 at 13:22

    Can anybody tell me for what this special sector is (it has to be setup in the Option Byte).

    If there is somewhere a decription pls specify where I can find it.

    Kurt

    Visitor II
    May 20, 2004
    Posted on May 20, 2004 at 11:46

    The Sector 0 can be used for in-application programming(IAP). The reset and interrupt vectors are located in Sector 0. Pls also refer ''flash programming manual'' . It can be downloaded from the same site.