Solution for measuring 4-20mA current non-invasively
I have a development project to monitor some information in an industrial environment in which sensors are built into the board. But I will need to add a modification that allows non-invasive readings of sensors already installed in companies that follow the 4 to 20ma reading standard. I thought about using the hall effect sensor, but as I haven't worked with this technology yet I still have doubts as to whether I would be able to take accurate readings within this current range. It would also be possible to use current sensors with Rsense, but it would be invasive. Could you help me choose a sensor for this application?