[Solved]Calc board based on STCH02. Assemble it, but it does not work properly!
Worked in burst mode from 50V HV, then lower output voltage till 120VAC input, and almost totally powered off when input VAC above 135V. The ZCD resistive divider is 82 kOhm and 12 kOhm. Transfomer has 100 turns, 7 and 7 turns respectively. Lpri about 2.7 mHn. I tried 1.3 mHn and 0.9 mHn too. The same results. Why?
Did anyone have some problems like that? Is anyone know how to calc an impulse power transformer for STCH02 design?