Skip to main content
Visitor II
September 19, 2023
Question

Somebody know this ic?

  • September 19, 2023
  • 1 reply
  • 3454 views

Hi again to everyone!

I want to know, if somebody know something about this ic´s in the attached pictures (one it´s labeled: "a34 2248", and the other is: "2057 wow1", both in smd structure).

It is used to switch  beetwin two hdmi signals.

I´ve searched about they, without luck...

Thanks in advice!!!

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 19, 2023

    The two components are in package variants QFN18 and TSSOP6/SOT23-6 or similar designations. Apart from protection arrays, however, STMicroelectronics does not offer any devices that have anything to do with HDMI, not even the components shown, so we cannot make any statement. But maybe one of the community users is in a position to do so?

    Good luck!
    /Peter

    angeliranAuthor
    Visitor II
    September 19, 2023

    Thx for answer @Peter BENSCH , i thing it´s a multiplexor ic, it only switch btween two signals pins.