Skip to main content
Visitor II
January 7, 2007
Question

SPI bus speed

  • January 7, 2007
  • 6 replies
  • 1196 views
Posted on January 08, 2007 at 00:19

SPI bus speed

    This topic has been closed for replies.

    6 replies

    Visitor II
    March 8, 2006
    Posted on March 08, 2006 at 10:49

    Hello,

    I want to transfer data with a MMC card.

    What is the maximum speed in Mhz of SPI bus on STR710 chip?

    Thank you

    :)

    Visitor II
    March 8, 2006
    Posted on March 08, 2006 at 11:17

    I want to know the maximum BSPI bus speed in master mode (in Mhz).

    Thanks

    Visitor II
    March 8, 2006
    Posted on March 08, 2006 at 11:44

    Hi,

    Each of the two SPIs allow full duplex, synchronous communications with external devices,

    master or slave communication at up to 5.5Mb/s in Master mode and 4 Mb/s in Slave mode.

    Hich :p

    Visitor II
    March 8, 2006
    Posted on March 08, 2006 at 11:58

    Thank you very much, but I want to know the max speed of BSPI bus in Mhz.

    -> APB1 /6 in master mode = X Mhz ?

    Visitor II
    January 5, 2007
    Posted on January 05, 2007 at 11:57

    Quote:

    On 08-03-2006 at 16:14, Anonymous wrote:

    Hi,

    Each of the two SPIs allow full duplex, synchronous communications with external devices,

    master or slave communication at up to 5.5Mb/s in Master mode and 4 Mb/s in Slave mode.

    Hich :p

    I would to have a little precision : is 4 Mb/s the maximum speed in Slave mode? Is'n it 4.096MHz ?

    Thanks for reply,

    Regards,

    Visitor II
    January 7, 2007
    Posted on January 08, 2007 at 00:19

    It looks like 4.096 mhz is the clock frequency. Did I say the clock frequency. The STR should be running at a higher speed using the PPL. Read the manual on the OSC, PPL and SPI.