Skip to main content
Visitor II
April 7, 2021
Question

SPI communication between Eval l9963 with on board MCU and an esp32.

  • April 7, 2021
  • 0 replies
  • 933 views

So i have a few questions regarding the SPI communication

1) Is the burst commands mentioned in the L9963E datasheet applicable with Eval-l9963 also?

2) While sending the 40 bit command (single access and burst command) i'm only getting a integer value of 200 (in my esp32)is there something i'm doing wrong here?

3)is there any fixed commands to receive the voltage and temperature data?if so anyone can comment it down?

i'm a beginner in the coding area . thanks in advance.

    This topic has been closed for replies.