Skip to main content
Visitor II
May 30, 2006
Question

spi problem str7xf

  • May 30, 2006
  • 2 replies
  • 697 views
Posted on May 30, 2006 at 07:35

spi problem str7xf

    This topic has been closed for replies.

    2 replies

    bljiAuthor
    Visitor II
    May 25, 2006
    Posted on May 25, 2006 at 08:53

    Hi

    I have a problem in SPI to have communication work from slave->Master.

    Use str7 library.

    BSPI_BSPI0Conf(ENABLE);

    BSPI_Init ( BSPI0 ) ;

    BSPI_ClockDividerConfig ( BSPI0, 6);

    BSPI_Enable ( BSPI0 , ENABLE );

    BSPI_MasterEnable ( BSPI0,ENABLE);

    BSPI_ClkActiveHigh(BSPI0,ENABLE);

    BSPI_ClkFEdge(BSPI0,DISABLE);

    BSPI_8bLEn(BSPI0,ENABLE);

    BSPI_TrFifoDepth(BSPI0,9);

    BSPI_RcFifoDepth(BSPI0,3);

    I do have same functions for slave except

    BSPI_MasterEnable ( BSPI0,DISABLE);

    When I send byte from slave-> master is not working. But Master->slave works.

    Also I have another issue in strxf I am not able to make spi1 function as master and spi0 slave.

    Thanks

    blji

    Visitor II
    May 30, 2006
    Posted on May 30, 2006 at 07:35

    Hi, I think that you posted your question in the wrong forum, as it is related to ARM STR7 nad not ST7 you should have posted it in the ''ARM7 STR7'' forum:

    http://mcu.st.com/mcu/modules.php?mop=modload&name=Splatt_Forums&file=viewforum&forum=17

    Regards