Anyone know how to configure DMA-controller and SSP0 in Slave-Mode to use DMA for Tx & Rx synchronous?
I'll try to communicate with a SPI-Master and want to use DMA to transfer the Data between SSP0 and memory. SPI-communication seems to work. I'll see communication on a oscilloscope. If I use DMA, I receive correct data. But the transmit data is shifted about 8 Bytes. Here is the DMA configuration:void DMA_Configuration(void) { DMA_StructInit(&DMA_InitStructChannel0); DMA_StructInit(&DMA_InitStructChannel1); DMA_DeInit(); DMA_Cmd(ENABLE); DMA_SyncConfig((TUINT16)(DMA_SSP0_TX_Mask | DMA_SSP0_RX_Mask), ENABLE); /* DMA Channel 0 */ DMA_StructInit(&DMA_InitStructChannel0); DMA_InitStructChannel0.DMA_Channel_LLstItm = 0; /*No linked lists used*/ DMA_InitStructChannel0.DMA_Channel_SrcAdd = (TUINT32)(&SSP0->DR); /*Source address*/ DMA_InitStructChannel0.DMA_Channel_DesAdd = (TUINT32)&Test_SspRcvProfiBuf.SspRcvbytes[0]; /*Destination address*/ DMA_InitStructChannel0.DMA_Channel_SrcWidth = DMA_SrcWidth_Byte; /*Source width of one byte*/ DMA_InitStructChannel0.DMA_Channel_DesWidth = DMA_DesWidth_Byte; /*Destination width of one byte*/ DMA_InitStructChannel0.DMA_Channel_DesBstSize= DMA_DesBst_4Data; /* Initialize The Burst Size for the Destination */ DMA_InitStructChannel0.DMA_Channel_FlowCntrl = DMA_FlowCntrl2_DMA; /*The flow controller is the DMAC, Transfer Type: Peripheral-to-memory */ DMA_InitStructChannel0.DMA_Channel_Src = DMA_SRC_SSP0_RX; DMA_InitStructChannel0.DMA_Channel_TrsfSize = 183; /*Transfer size */ DMA_ChannelDESIncConfig (DMA_Channel0, ENABLE); /*We increment the destination not the source*/ DMA_ITConfig(DMA_Channel0, ENABLE); /*Enable the Terminal Count interrupt*/ DMA_ITMaskConfig(DMA_Channel0, (TUINT16)DMA_ITMask_ITC, ENABLE); DMA_Init(DMA_Channel0, &DMA_InitStructChannel0); /* DMA Channel 1 */ DMA_StructInit(&DMA_InitStructChannel1); DMA_InitStructChannel1.DMA_Channel_LLstItm = 0; /*No linked lists used*/ DMA_InitStructChannel1.DMA_Channel_SrcAdd = (TUINT32)&Test_SspSndProfiBuf.SspSndbytes[0]; /*Source address*/ DMA_InitStructChannel1.DMA_Channel_DesAdd = (TUINT32)((&SSP0->DR)); /*Destination address*/ DMA_InitStructChannel1.DMA_Channel_SrcWidth = DMA_SrcWidth_Byte; /*Source width of one byte*/ DMA_InitStructChannel1.DMA_Channel_DesWidth = DMA_DesWidth_Byte; /*Destination width of one byte*/ DMA_InitStructChannel1.DMA_Channel_SrcBstSize= DMA_SrcBst_4Data; /* Initialize The Burst Size for the Source*/ DMA_InitStructChannel1.DMA_Channel_FlowCntrl = DMA_FlowCntrl1_DMA; /*The flow controller is the DMAC, Transfer Type: Memory-to-peripheral */ DMA_InitStructChannel1.DMA_Channel_Des = DMA_DES_SSP0_TX; DMA_InitStructChannel1.DMA_Channel_TrsfSize = 183; /*Transfer size */ DMA_ChannelSRCIncConfig (DMA_Channel1, ENABLE); /*We increment the source not the destination*/ DMA_ITConfig(DMA_Channel1, ENABLE); /*Enable the Terminal Count interrupt*/ DMA_ITMaskConfig(DMA_Channel1, (TUINT16)DMA_ITMask_ITC, ENABLE); DMA_Init(DMA_Channel1, &DMA_InitStructChannel1); } Here the SSP0 configuration:void SSP0_Configuration(void) { SSP_InitTypeDef SSP_InitStructure; /* Init-Struct der SSP */ TUINT32 k; SSP_DeInit(SSP0); SSP_StructInit(&SSP_InitStructure); /* SSP0 initialization */ SSP_InitStructure.SSP_FrameFormat = SSP_FrameFormat_Motorola; SSP_InitStructure.SSP_Mode = SSP_Mode_Slave; SSP_InitStructure.SSP_CPOL = SSP_CPOL_Low; /* CPOL = 0 */ SSP_InitStructure.SSP_CPHA = SSP_CPHA_2Edge; /* CPHA = 1 */ SSP_InitStructure.SSP_DataSize = SSP_DataSize_8b; SSP_InitStructure.SSP_SlaveOutput = SSP_SlaveOutput_Enable; SSP_Init(SSP0, &SSP_InitStructure); /*Enable SSP0 DMA request*/ SSP_DMACmd(SSP0, (TUINT16)SSP_DMA_Transmit, ENABLE); SSP_DMACmd(SSP0, (TUINT16)SSP_DMA_Receive, ENABLE); /* SSP0 enable */ SSP_Cmd(SSP0, ENABLE); } DMA Transfer is started in an ISR for an external IRQ, which is parallel connected to NSS from SSP0 (chip select).Thanks in advance Heiko [ This message was edited by: heikomasiero on 26-06-2008 14:54 ] [ This message was edited by: heikomasiero on 26-06-2008 14:55 ]