Skip to main content
Visitor II
February 9, 2005
Question

ST NAND flash source code help

  • February 9, 2005
  • 1 reply
  • 644 views
Posted on February 09, 2005 at 09:09

ST NAND flash source code help

    This topic has been closed for replies.

    1 reply

    smittAuthor
    Visitor II
    February 9, 2005
    Posted on February 09, 2005 at 09:09

    Hi.

    Im develomping an MP3 player using the source code from ST´s NAND flash memory example. I was actualy rather amased over how much code was needed for a memory stick.

    My problem is that I need to add a function to the source code. I have understod that I should call my own functions from the appli.c file. But there is no help file / app. note for this source code, therefore Im having truble understanding it. I need to get a mp3 file from the nand flash but doesnt understand which function I should call on from the MAL(?) library.

    I also need some kind of get filelist function that returns directories and filenames stored in the nand memory.

    I would appreciate any help. Or links to dokuments and Appnotes clarifying this.

    Best regards

    Fredrik