if i use the EBC in DeMuxed bus in 64 MHZ can i choose the ALECTL to be 0 -> this causes (according to the data sheet) the time of t5(ALE High time) to be -1.5ns approx? is that leagal? i want to do this to achive the max out of the part. thanks, Uri.
if i want to squize the max performance out of the ST10F276 and i use the Demuxed bus, this time is of no importance to me, can i use the ALECTL = 0 ? or that will cause the device to malfunction? Regards, Uri.