what are the software debugging options we have if we use the tasking compiler and the ST10F276? are we bound to use the Rom-monitor (cross-view)? if so can we put break points in the iFLASH and xFLASH? if every thing else fails is there a recommended ICE to use? thanks, Uri.
1/ what are the software debugging options we have if we use the tasking compiler and the ST10F276? Please have a look to the enclosed AN provided by Tasking for details about debugging settings. 2/ Are we bound to use the Rom-monitor (cross-view)? No, you are not bound to use the ROM monitor! You have the choice between RAM monitor(load your code in an external RAM) and ROM monitor(load your code in the flash). 3/ if so can we put break points in the iFLASH and xFLASH? I am not sure that using Cross View to load code in the flash allows putting breakpoints. I will check this point and tell you. 4/if every thing else fails is there a recommended ICE to use? You can use an ICE provided by Nohau. Please refer to the document available on the following link: http://www.nohau.com/parts_lists/emst.pdf Regards, Najoua. [ This message was edited by: Najoua on 08-03-2006 13:44 ] [ This message was edited by: Najoua on 08-03-2006 13:46 ]
________________
Attachments : TaskingAN.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0L6&d=%2Fa%2F0X0000000bXd%2FOVujbFTriLkwx6HaP2ocT6Ap8hhwFr25pCjj1vQYKEE&asPdf=false