When trying to program st6265 with the starter kit and Intel hex code generated by Realizer 2 I am receiving verify error message at address 0080. Previously have successfully programmed chips with the same code and starter kit but on a different computer.My prenet computer is a laptop. Can successfully read from chips and blank check and verify but cannot verify when hex file is opened or program the chip. Has anyone any bright ideas?
THE PROBLEM WAS SIMPLY THAT THE VOLTAGE I WAS USING (12V) WAS BELOW THE RECOMMENDED VALUE OF BETWEEN 16-20V. SIMPLE MISTAKE BUT BEWARE![ This message was edited by: jaycee on 12-12-2003 16:51 ]
The starter kit compatibility upto some extent depend on PC to PC. The problem in your case could be because of high speed of your Laptop. Also use the latest verion of Window eprommer (Winee 4.0.3) and then try. It is free available on internet(www.stmcu.com).