Skip to main content
Visitor II
August 11, 2005
Question

ST7 Bootloader

  • August 11, 2005
  • 2 replies
  • 745 views
Posted on August 11, 2005 at 11:01

ST7 Bootloader

    This topic has been closed for replies.

    2 replies

    vikramAuthor
    Visitor II
    August 11, 2005
    Posted on August 11, 2005 at 07:29

    The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6po&d=%2Fa%2F0X0000000bwR%2FTNjsPerLd.8THGp.O_y9VSNnXDYoCFIvBk5CIxaboBM&asPdf=false
    Visitor II
    August 11, 2005
    Posted on August 11, 2005 at 11:01

    Vikram,

    your problem is pretty complex (as well as everything else related to IAP), so please consider what I write below as ''suggestions'' only; I have not tried any of that on my PC.

    The easiest solution is probably to not use initialised variables in the application; you can initialise them ''by hand'' at the beginning of main() and get the same result.

    If this is not acceptable, there are a couple other possible options:

    - have the startup part of the bootloader initialise the variables of the application (and not of the bootloader itself); for this you need to replace __idesc__ with some other variable at an absolute address in sector 2

    - include the startup in the application as well (and not only in the bootloader)

    On a side note, looking at your linker files, I think there's an easier way to redirect the interrupt vectors, see ''implementing a skip-jump table'', a few posts below.

    Hope it helps.

    Regards,

    Luca