Skip to main content
Visitor II
March 28, 2006
Question

ST7FLite with internal RC-oscillator

  • March 28, 2006
  • 2 replies
  • 818 views
Posted on March 28, 2006 at 06:00

ST7FLite with internal RC-oscillator

    This topic has been closed for replies.

    2 replies

    Visitor II
    April 26, 2005
    Posted on April 26, 2005 at 09:00

    Hi All,

    I've a special question in using the internal RC-oscillator of the ST7FLite2X.

    The manual says:

    Internal RC Oscillator

     

    In this mode, the tunable 1%RC oscillator is used

     

    as main clock source. The two oscillator pins have

     

    to be tied to ground.

    My question is: What can happen, if I don't connect the two pins to ground? Fact is, that I leave them open - to an alternative option with a quartz - with two 22nF capacitors and can't recognize any fault.

    Thanks for any suggestions

    WoRo

    Visitor II
    March 28, 2006
    Posted on March 28, 2006 at 06:00

    I'm launching my question again, hoping that finally one of the so called moderators will bother to give an answer, or any other in this forum is able to do so.

    Waiting again and thanks in advance

    WoRo