Skip to main content
Visitor II
May 21, 2003
Question

ST7Lite

  • May 21, 2003
  • 3 replies
  • 925 views
Posted on May 21, 2003 at 06:49

ST7Lite

    This topic has been closed for replies.

    3 replies

    pichetAuthor
    Visitor II
    May 18, 2003
    Posted on May 19, 2003 at 01:37

    Hello Anyboby

    ST7Lite2 Current

    I'm using an ST7lite2 and I need to save as much current as possible without an increase to cost.

    The LVD detection is taking 0.2mA - Is there a better solution?

    or should I use a external regulator with low voltage detection (But this will add to the cost of the final production)

    JOM

    Visitor II
    May 19, 2003
    Posted on May 19, 2003 at 12:00

    hello,

    You can reduce the power consumption by using different power saving modes e.g. halt etc. . Its usage depends up on your application means which peripheral/s you want to use and other configuarations.

    [ This message was edited by: Ranjeet on 19-05-2003 15:30 ]
    Visitor II
    May 21, 2003
    Posted on May 21, 2003 at 06:49

    Don't forget also to configure all the unused I/Os as output at 0, to switch off all the unused peripherals, to switch off the ADC between 2 conversions if you don't need continuous conversions,...