My customer is using now the ST7Lite for one of his application and he need an accurate communication between the RS232 and he can't use the calibration so i gave him the ST7Superlite for this application . 1 . Can he write the code in the ST7Lite with the Softec Board and then transfer it to the SuperLite ? 2 . When i can get samples of the ST7SuperLite? Latino Israel
Why can't your customer use the 'FLITE for RS232? The only problem with the internal RC value is when the supply voltage changes. I have sw uart running on the 'FLITE0 with no problem Simon Anglia