Requesting a stop will clear the event flags 2. In your case, it is up to the ST9 to acknowlede for the reception. So, if the byte is correctly received, there is BTF and acknowledge events. Otherwise, no BTF and the ST9 will not acknowledge 3. No delay 4. No question ! Skywalker
Thank you for responding. I have since been able to write and read back bytes from the EEPROM, but still am having issues. I attached my code. It basically is the same as the previous sample code, except I broke the flag checking in i2_isr() function up into their specific interruptus. In other words, I am only testing for conditions that may have caused the specific interrupts:
1. Ok. 2. In my attached code at first I kept track of the bytes received and when there was only 1 byte left, I disable the ACK so that the next byte received (the last byte) does not get an ACK, and a STOP is then generated instead. Otherwise, since the interrupt is generated because the ACK was sent (according to data sheet), I would expect the EEPROM to send another byte because it was acknowledged. However, I remove this section and replaced it with a STOP and it works ok. I'm not sure why it works like this though. Does anyone understand why? 3. In the attached code, if I remove the delay in main() between the write and the read, I do not get the correct data read. I thought removing the delay would work because the START bit would be set and then an AF would be generated. In the error interrupt, I set the START bit...this would repeat until the write cycle was finished. At that time the EEPROM would send an ACK and then the process would proceed. Does not work though. I get a lot of AFs, but no data read? 4. I am questioning the ability of the peripheral to send a repeated start. It seems like this is not possible. In other words, you can not generate a START before generating a STOP when a previous START has been sent. An example of this is the random read in the previous attached file. Does anyone agree? In my code I too ended up generating a STOP after writing the memory address that I want to read from. This seems to work. I'm wondering if it cause the EEPROM to perform a longer read cycle by sending it a STOP like that? I also noticed that putting break points into the code cause different results than if the read and write cycles are allowed to complete. this is why I have the variables in the code that count the bytes, control words, and address sent. Note: On my same application board I am using a real time clock with an I2C interface (ST M41T00). In order to get it to work, I had to un-remark the two lines of code (described in (2) above ) that disabled the interface from generating an ACK before the last byte read. In other words, the M41T00 did not work unless the ACK was disabled before receiving the last byte. [ This message was edited by: Smiles on 06-04-2003 00:17 ]