Skip to main content
Visitor II
February 19, 2003
Question

ST90158 epb schematics

  • February 19, 2003
  • 3 replies
  • 960 views
Posted on February 19, 2003 at 15:35

ST90158 epb schematics

    This topic has been closed for replies.

    3 replies

    piresjojoAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    Hello,

    A customer is porgramming without pb a lot of st90158 with ST90158EPB board, but when he received news micros, and tried to program it the programation failed. But on an other board the programation was succeeded.

    Is there two type of ST90158EPB board ?

    Is it possible to have the schématics of the ST90158-EPB ?

    Thanks

    regards

    jorge
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    Find attached ''mb276b.pdf'' epb schematics. For ST90E158LV low voltage devices (3.3V) the power supply has been trimmed on EPB in August 1999. The modifications was:

    1) change resistor R7 from 2.00K to 1.5K

    2) change resistor R12 from 3.9K to 2.2K
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:33

    Hello Jorge,

    Regarding the ST90158-EPBJ board, I have recently acquire one which has a V2.00 tag on it. Based on tarayre's comment and since this board has been checked by ST in july 2002 (see product delivery form provided with the programmer), it must be the latest available revision.

    It will be a big improvement if this web site could provide latest version number for each ST9 tools (programmer and emulator).

    Breizh

    [ This message was edited by: Breizh on 19-02-2003 20:20 ]