STA540 BTL parallel
Dear technical team
I'm designing a triamped system with the STA540 , in fact it uses two STA540's per unit.

I've divided the system in one STA amplifying stereo treble and mid, and other STA for bass amplifier, but given that bass channel is not stereo (has the sum of L and R bass, I'd like to know if I may parallell channels 1 || 3 and 2 || 4 for a single bridge amplifier, instead of using only one bridge (1-2 or 3-4)
Can this chip operate with parallell channels? If it can, is it okay to use the channels that I've listed, or there is a better channel pairing?
Best
Ignacio