Skip to main content
Visitor II
January 13, 2005
Question

startup routine

  • January 13, 2005
  • 2 replies
  • 787 views
Posted on January 13, 2005 at 10:27

startup routine

    This topic has been closed for replies.

    2 replies

    Visitor II
    December 9, 2004
    Posted on December 09, 2004 at 06:09

    Hi,

    Is anybody able to explain what does the statup routine provided by the Metrowerks Codewarrior C compiler ?

    I'm using it with the inDART-STX and, in debbug mode,when I ''run'' the code directly at statup, it bugs and say ''communication problem'' when I stop it.

    On the other hand, when I change the source file and make ''run to cursor'' in the ''main'' routine or if I run it through ''Steps'', it works properly ! :o

    Does anybody already had this problem ? Is it comming from the startup routine or am I making mistakes in the memory configuration ?

    Thanks for your help.

    Visitor II
    January 13, 2005
    Posted on January 13, 2005 at 10:27

    Depending of th type of Flash on your ST7 (XFlash and HDFlash) and if the ST7 is equiped with the Debug Module the limitations of the ICD are different.

    Last running or stepping with InDart are in fact two different way of operating.

    The best is to contact Softec support (support@softecmicro.com) which will be pleased to help resolve your issue.

    Best regards,

    Alain