Skip to main content
Visitor II
August 20, 2003
Question

stkit st622x win2000 problem

  • August 20, 2003
  • 3 replies
  • 833 views
Posted on August 20, 2003 at 06:57

stkit st622x win2000 problem

    This topic has been closed for replies.

    3 replies

    wojciech2Author
    Visitor II
    August 11, 2003
    Posted on August 11, 2003 at 05:36

    Bad work on the win2000, cannot communicate with the device. With win98 is OK. Software ''Windows Epromer'' version 4.02 or 3.3, both is not working.

    Can anybody help me?
    Visitor II
    August 11, 2003
    Posted on August 11, 2003 at 10:20

    See text below from the ST6 Windows Epromer 4.0.2 Release Note.

    Make sure the NT parallel port driver is installed. This driver installs itself if not detected at the end of the windows epromer install. You should propably reinstall your windows eprommer software.

    --------------------------------------------------------------

    ST6 Windows Epromer can be installed on PCs and compatibles running with Windows ® 95,

    Windows ® 98, Windows ® 2000 or Windows ® NT ® 4.0 operating systems.

    Note: Installing WINDOWS EPROMER on a Windows ® NT or Windows ® 2000 machine for hardware

    programming tools which use the parallel port on your host PC, will trigger the installation of the NT

    Driver “STM Parallel Driver� if it has not yet been installed. In this case, administrator rights are

    required.
    wojciech2Author
    Visitor II
    August 20, 2003
    Posted on August 20, 2003 at 06:57

    I installed this driver and reinstalled eprommer software. Is still not working.