STlink can't connect to device [stm32f103c8t6 bluepill]
I recently got another bluepill board (stm32f103c8t6) to replace the old board, and I could not connect to it using stlink. Using OpenOCD:
Open On-Chip Debugger 0.12.0+dev-00600-g090b431b1 (2024-09-13-19:14) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J45S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.262724
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x2ba01477
Info : [STM32F103C8Tx.cpu] Cortex-M3 r2p0 processor detected
Info : [STM32F103C8Tx.cpu] target has 6 breakpoints, 4 watchpoints
Info : [STM32F103C8Tx.cpu] Examination succeed
Info : starting gdb server for STM32F103C8Tx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32F103C8Tx.cpu:
C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.3.0.202411041438/resources/openocd/st_scripts/gdb_helper.tcl:18: Error: TARGET: STM32F103C8Tx.cpu - Not halted
in procedure 'gdb_attach_hook' called at file "C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.3.0.202411041438/resources/openocd/st_scripts/target/stm32f1x.cfg", line 184
in procedure 'first_gdb_attach_hook' called at file "C:/ST/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.3.0.202411041438/resources/openocd/st_scripts/gdb_helper.tcl", line 18
Info : device id = 0x10010414
Info : flash size = 256 KiB
Warn : GDB connection 1 on target STM32F103C8Tx.cpu not halted
undefined debug reason 8 (UNDEFINED) - target needs reset
shutdown command invoked
Info : dropped 'gdb' connection
Does anyone know what's wrong with the board?? The stlink device is detected properly, but it cannot verify the st device.