Hi Mihai,
In short 1.25V are a limitation on inside comparator present in this family products, as specified in pag 32 (table 14) of datasheet (https://www.st.com/resource/en/datasheet/stnrgpf01.pdf)
So every time user have necessity to compare a signal using internal comparator, the pin should have following range 0-1,25Volts.
This is the golden rule, in solution proposed, applied on
- Input Voltage Sensing Circuit,
- Output Voltage Sensing Circuit,
- Output Current Sensing Circuit,
where output go directly to a STNRGPF01's pin for comparision.
On the contrary on Input Current Sensing Circuit, the output of this module is a input for PI regulator so only in this case we can use a different target voltage according to the IC used in the Current Control Loop (https://www.st.com/resource/en/datasheet/lmv321.pdf).
The two resistors R58 and R62, between PI's output and OUT_PIN, give a scale factor of 0.635 that ensure the correct voltage on OUT_PIN pin.
For further information on the proposed solution, it is also possible to refer to the following link, which shows a case of real use for STNRGPF01.
https://www.stmicroelectronics.com.cn/content/st_com/en/products/evaluation-tools/solution-evaluation-tools/psu-and-converter-solution-eval-boards/steval-ipfc01v1.html
I hope my answer has been exhaustive.
Regards.
Carmelo.