Skip to main content
Visitor II
June 21, 2004
Question

STPC ConsumerII + WinCE4.2 + HD + Floopy

  • June 21, 2004
  • 2 replies
  • 759 views
Posted on June 21, 2004 at 13:27

STPC ConsumerII + WinCE4.2 + HD + Floopy

    This topic has been closed for replies.

    2 replies

    Visitor II
    June 21, 2004
    Posted on June 21, 2004 at 06:27

    Dear heartness people,

    I am using STPC ConsumerII Eva BD and WinCE4.2 OS. I install hard disk on IDE and floopy on the bus. The hard disk and floopy can work for CEPC and hard disk can boot from nk.bin. And I had added the ''ATAPI PCI/IDE Storage Bolck driver'' and ''FAT File System'' into my plafform(follow the WinCE how to topic). But why I can't find HD and floopy after WinCE OS start up?

    Is there any one can tell me how to setup so that I can find HD and floopy in WinCE4.2 environment?

    Thank you very much!
    Visitor II
    June 21, 2004
    Posted on June 21, 2004 at 13:27

    G'day

    I have just a CompactFlash which is connected thru IDE (master on primary IDE). But the setting for the IDE device should be similar. Please check your platform.reg entry about the IDE device entries, they should be similar like mine.

    Because my system has a hive based registry, there are hive entries. Maybe they are not required in your system.

    Chris

    *** platform.reg ***

    ; 2003-07-10: begin CompactFlash settings

    ;**************************************************************

    ; Registry settings for IDE

    ;**************************************************************

    ; has to be in the hive boot section to

    ; enable the access to the CompactFlash

    ; during boot-prozess

    ; HIVE BOOT SECTION

    IF BSP_NOIDE !

    [HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Atapi]

    ''Prefix''=''IDE''

    ''Dll''=''atapi.dll''

    ''FSD''=''fatfsd.dll''

    ; io bases and leght for primary and secondary

    ''IoBase''=multi_sz:''1f0'', ''3f4'', ''170'', ''374''

    ''IoLen''=multi_sz:''8'', ''4'', ''8'', ''4''

    ''Settings''=dword:2

    ''Legacy''=dword:1

    ''IClass''=multi_sz:''{CDDC3621-3512-4b3f-BB6F-B4DD5E061795}''

    ''Order''=dword:0

    ''Index''=dword:1

    ; ''Flags''=dword:1000

    ; IDE Primary master

    [HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Atapi\Device0]

    ''Irq''=dword:0e

    ''Prefix''=''DSK''

    ''Dll''=''atapi.dll''

    ''DeviceId''=dword:0

    ''Ioctl''=dword:4

    ''ConfigEntry''=''GenericConfig''

    ''IClass''=multi_sz:''{A4E7EDDA-E575-4252-9D6B-4195D48BB865}''

    ; ''Flags''=dword:1000

    ; IDE secondary master

    ;[HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Atapi\Device2]

    ; ''Irq''=dword:0f

    ; ''Prefix''=''DSK''

    ; ''Dll''=''atapi.dll''

    ; ''DeviceId''=dword:2

    ; ''Ioctl''=dword:4

    ; ''ConfigEntry''=''GenericConfig''

    ; ''IClass''=multi_sz:''{A4E7EDDA-E575-4252-9D6B-4195D48BB865}''

    ; ; ''Flags''=dword:1000

    [HKEY_LOCAL_MACHINE\System\StorageManager\FATFS]

    ''CacheSize''=dword:ffffffff

    [HKEY_LOCAL_MACHINE\System\StorageManager\Profiles\HDProfile]

    ''Name''=''IDE Hard Disk Drive''

    ''Folder''=''CompactFlash''

    [HKEY_LOCAL_MACHINE\System\StorageManager\Profiles\HDProfile\FATFS]

    ''MountFlags''=dword:2

    ''EnableCacheWarm''=dword:0

    ENDIF BSP_NOIDE !

    ; END HIVE BOOT SECTION

    ; @CESYSGEN ENDIF CE_MODULES_ATAPI

    ;: end CompactFlash settings

    [ This message was edited by: chris_s on 21-06-2004 16:59 ]