Skip to main content
Visitor II
January 11, 2023
Question

STPS2150A ? X-ray射线照射,内部构造 ? ?

  • January 11, 2023
  • 2 replies
  • 1356 views

X irradiation was done on this product, and it was found that the position of the arrow was inconsistent. The same batch and the same plate of material were compared. What is the reason for this? Does it affect the performance use0693W00000Y7wS8QAJ.png

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    January 11, 2023

    Welcome, @应姣 �?�​, to the community!

    Now, if you look closely at the X-ray, you will notice that the components marked in red are mirrored, i.e. turned upside down.

    Regards

    /Peter

    应李.1Author
    Visitor II
    January 11, 2023

    Dear

    I don't quite understand. Does this mean that our operation is reversed? Does this situation affect the use of

    [private data removed by moderator]

    Technical Moderator
    January 11, 2023

    Unfortunately, you can't see on the Xray where the STPS2150s were photographed, i.e. whether they are on a board or just xrayed somewhere.

    If you mirror the components outlined in red, i.e. turn them upside down using the graphic editor, as can be seen in the example at the top right, then they look normal, right?

    0693W00000Y7xJCQAZ.png

    应李.1Author
    Visitor II
    January 11, 2023

    My device pendulum is exactly the same, 9 devices a picture taken down, I asked why through a batch of the same plate in the same direction taken out of the internal structure is not the same0693W00000Y7xBwQAJ.png

    Technical Moderator
    January 11, 2023

    Ah, now I see. That's an interesting observation that only the quality department can answer. The best thing to do is to discuss this with your distributor, where you bought the parts, and ask them for a statement.

    Regards

    /Peter