Skip to main content
Visitor II
December 7, 2007
Question

STR712FR2: problems with interrupts while running from RAM...

  • December 7, 2007
  • 2 replies
  • 774 views
Posted on December 07, 2007 at 10:11

STR712FR2: problems with interrupts while running from RAM...

    This topic has been closed for replies.

    2 replies

    Visitor II
    December 4, 2007
    Posted on December 04, 2007 at 07:41

    Dear All,

    I have encounered a problems with interrupts while running code from RAM...

    Environment:

    Keil uVision 3.55a and MDK 3.15b

    I took an example from Examples\ST\STR71xLib\Tim\OCMP and changed it in the way to work in RAM.

    What i see is that Timer 3 output compare function pin triggers but interrupt routine doesn't work (there are no port pins toggling)...

    When i run it in debug mode (using the internal uVision debugger) all seems to be working...

    Does anybody encounter with such problems before?

    I would be very appreciated for your help.

    P.S.Source code i'm experimenting with is attached for your consideration...

    Thank you.

    ________________

    Attachments :

    OCMP.ZIP : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1NS&d=%2Fa%2F0X0000000bmC%2FqFJqRlnvhC9zyQOZAYNG8KIfJK7mU4OgE2s.E_r4d7Q&asPdf=false
    Visitor II
    December 7, 2007
    Posted on December 07, 2007 at 10:11

    I have an STR710 interrupt example running from RAM and the porject setting is different than yours. you can check also the boot pin on your board. I attached my setting. Hope this helps you,

    Cheers,

    Chris.

    [ This message was edited by: christophe.beyen on 07-12-2007 14:43 ]

    ________________

    Attachments :

    project-setting.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtQZ&d=%2Fa%2F0X0000000aPs%2Fmnzo5O4R9sLjnD3M8kBe.y98FobZG6VD6elw6H1kIUQ&asPdf=false