Skip to main content
Visitor II
May 15, 2007
Question

STR9-DONGLE

  • May 15, 2007
  • 5 replies
  • 1058 views
Posted on May 15, 2007 at 03:48

STR9-DONGLE

    This topic has been closed for replies.

    5 replies

    yuhleonAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:43

    I'm trying STR-DONGLE source code , I download it from :

    http://mcu.st.com/mcu/inchtml.php?fdir=pages&fnam=str9_promoboard

    But I only have STR910-EVAL board , so I change the code in hw_config.h :

    #define STR9_EVAL

    //#define STR9_DONGLE

    Then use IAR to build this project . But occurs 1 error :

    Error[Pe167]: argument of type ''struct ip_addr'' is incompatible with parameter of type ''unsigned int'' D:\SourceCode\STR9 Dongle\FreeRTOS\Demo\ARM9_STR91X_IAR\lwip\api\BasicWEB.c 229

    I remove above error code , and download it to my STR9-EVAL .

    It cannot work .

    Does anyone have tried this code on STR9-EVAL ?

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:43

    You can find the last release of the code in this demo

    at

    http://www.freertos.org/

    yuhleonAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:43

    The demo project at

    http://www.freertos.org

    is for STR910-EVAL . There is no demo code for STR9-DONGLE .

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:43

    You are right,

    I addressed you to the FreeRtos project page

    where you can find the latest str91x porting.

    The porting is made on the str910eval.

    I don't understand if you have a str9dongle or

    a different board.

    In any case, the differences between these board

    are related to a different peripherals configuration...

    I use this RTOS in my own board withot problem.

    yuhleonAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:43

    The reason I want to use STR9-DONGLE demo code is that has lwIP , the FreeRTOS official demo project is using uIP .

    I want to use lwIP instead of uIP , so I would like to use STR9-DONGLE demo code for some reference .

    Thanks for your help .