Question
STR9 - Inrush current on the VDD supply
Posted on July 29, 2014 at 16:52
Hi,
I have a issue with the power supplies of my electronic board at start up of microcontroller STR912FAW47. Someone know the inrush current of microcontroller on VDD (1,8V) and VDDQ (3.3V) at power on? With an oscilloscope, it seems that the microcontroller starts to consume at the VDD treshold of 0,7V because I have an inrush current when the VDD supply is above 0,7V. Thanks, Jerome