i'm a new to use STR9- ARM with KEIL kit: STR91X-SK/KEI/A. When i startup the µVISION3 it stop loading with this error :''Eccezione WIn32 in armcc.exe'' I have ''Microsoft Windows XP Professional 2002 Service Pack 2'' original. Intel Pentium 4 CPU 2.53GHz Can you help me.....
I was recently getting this problem. Here are the steps I used to ''fix'' the problem:
1. I deleted all the .dep and .Bak files from the directory that my .Uv2 project file was in. 2. I also deleted all the listing files and output files (there was no need for me to keep them around anyway) 3. I then rebooted. 4. Opened up my .Uv2 file and was able to compile without problem.