Question
STR912 Partiry bit set Error.
Posted on April 09, 2014 at 13:48
hi.dear
i use to IAR compiler, default_form_lib_2.1_iar_5.30 library and jlink. it is my developer environment. my chip is STR912FAW44. first. i initialize UART2 set None parity bit. second. i change to UART2 set Even parity bit. i check registor by jlink. it is ok changed Even parity bit. but it was still operationg in non parity bit. next is my initialize UART1 and baud rate change C code. void UART1_Initial(void) { /* Enable the UART0 Clock */ SCU_APBPeriphClockConfig(__UART1, ENABLE); SCU_APBPeriphReset(__UART1,ENABLE); UART_DeInit(UART1); GPIO_StructInit(&GPIO_InitStructure); //Initialize the GPIO Init Structure parameters /*Gonfigure UART1_Rx pin GPIO3.2*/ GPIO_InitStructure.GPIO_Direction = GPIO_PinInput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Enable; GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1 ; GPIO_Init(GPIO3, &GPIO_InitStructure); /*Gonfigure UART1_Tx pin GPIO3.3*/ GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2 ; GPIO_Init(GPIO3, &GPIO_InitStructure); UART_InitStructure.UART_WordLength = UART_WordLength_8D; UART_InitStructure.UART_StopBits = UART_StopBits_1; UART_InitStructure.UART_Parity = UART_Parity_No ; UART_InitStructure.UART_BaudRate = 115200; UART_InitStructure.UART_HardwareFlowControl = UART_HardwareFlowControl_None; // no flow controll UART_InitStructure.UART_Mode = UART_Mode_Tx_Rx; UART_InitStructure.UART_FIFO = UART_FIFO_Disable; size 16 bytes, FIFO level 8 bytes */ UART_Init(UART1, &UART_InitStructure); UART_ITConfig(UART1, UART_IT_Receive | UART_IT_Transmit, ENABLE); VIC_Config(UART1_ITLine, VIC_IRQ, 5); VIC_ITCmd(UART1_ITLine, ENABLE); /* Enable the UART0 */ UART_Cmd(UART1, ENABLE); } void uart1_baudrate_set(INT32U baud) { UART_InitStructure.UART_WordLength = UART_WordLength_8D; UART_InitStructure.UART_StopBits = UART_StopBits_1; UART_InitStructure.UART_Parity = UART_Parity_Even ; switch(baud) { case BAUD_RATE_9600: case BAUD_RATE_19200: case BAUD_RATE_38400: case BAUD_RATE_57600: case BAUD_RATE_115200: UART_InitStructure.UART_BaudRate = baud; break; default : UART_InitStructure.UART_BaudRate = 115200; break; } UART_InitStructure.UART_HardwareFlowControl = UART_HardwareFlowControl_None; UART_InitStructure.UART_Mode = UART_Mode_Tx_Rx; UART_InitStructure.UART_FIFO = UART_FIFO_Disable; UART_Init(UART1, &UART_InitStructure); }I
can not
understand this situation
.
i want to solution.