Skip to main content
Visitor II
January 23, 2007
Question

STR912F44W CAN receiver not working

  • January 23, 2007
  • 2 replies
  • 603 views
Posted on January 23, 2007 at 07:07

STR912F44W CAN receiver not working

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:35

    hi Softy,

    >CAN-TX on port 5.1 is working (in Loopback-mode) but the receiver is not working in all modes

    Can you send the configuration (CAN and GPIO)you're using ?

    it seems that the GPIO configuration is not right because the loopback-mode is working ;)

    Waiting for your response

    best regards.

    :D

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:35

    The problem is: STR912F44W CAN node in silent-mode.

    CAN-TX on port 5.1 is working (in Loopback-mode) but the receiver is not working in all modes - also not in silent mode. FI2 is selected for RX buffer. Acceptance filter is set to the full range like the example does. Interrupt is enabled scu on port 5 is enabled - but no int occures. Any ideas? :o