Skip to main content
Visitor II
July 9, 2004
Question

stvd7 3.0 problem

  • July 9, 2004
  • 4 replies
  • 703 views
Posted on July 09, 2004 at 07:16

stvd7 3.0 problem

    This topic has been closed for replies.

    4 replies

    huaer2000Author
    Visitor II
    June 21, 2004
    Posted on June 21, 2004 at 07:43

    dear all,

    while I use Stvd7 3.0 simualtor to debug, there's a error message'' simulator error: unknown mcu name'' . I don't know why, coudl anyone help to explain it. attached pls find the whole directory zip file.

    mcuinterest

    ________________

    Attachments :

    stv73test.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzHO&d=%2Fa%2F0X0000000bTn%2FSmdKR6qSOsMlBf1jwasHX0mQlY4BmhS7GhlnA4SWEO4&asPdf=false
    Visitor II
    June 21, 2004
    Posted on June 21, 2004 at 12:42

    Hi mcuinterest,

    I've sent you a private message naming the author of the program. You should be able to find him from that.
    Visitor II
    June 21, 2004
    Posted on June 21, 2004 at 14:17

    Its look like this device is not simulated by stvd3, try using another device such as ST72324J4.

    Also you have not defined enough interrupt vectors to cover the vector section: FFE0-FFFF.

    It should be

    segment 'vectit'

    DC.W int_catch

    DC.W int_catch

    DC.W int_catch ; FFE4-FFE5h AVD

    DC.W int_catch ; FFE6-FFE7h SCI

    DC.W int_catch ; FFE8-FFE9h TimerB

    DC.W int_catch ; FFEA-FFEBh TimerA

    DC.W int_catch ; FFEC-FFEDh SPI

    DC.W int_catch ; FFEE-FFEFh not used

    DC.W int_catch ; FFF0-FFF1h External Interrupt 3

    DC.W int_catch ; FFF2-FFF3h External Interrupt 2

    DC.W int_catch ; FFF4-FFF5h External Interrupt 1

    DC.W int_catch ; FFF6-FFF7h External Interrupt 0

    DC.W mcc_int ; FFF8-FFF9h MCC/RTC/CSS

    DC.W int_catch ; FFFA-FFFBh Not Used

    DC.W int_catch ; FFFC-FFFDh TRAP Software Interrupt

    DC.W main ; FFFE-FFFFh RESET

    or change section to FFE4-FFFF

    Regards

    sjo
    Visitor II
    July 9, 2004
    Posted on July 09, 2004 at 07:16

    With the new 3.0.1 release, you can see, when selecting the MCU, which device is supported by the simulator and which is not.

    Emmanuel.