I need to program a UPSD3234BV part in system via the JTAG port. As with other ISP devices, I generated a SVF file from the OBJ. I have the following questions: 1. While I understand the functionality of TERR and TSTAT I cannot see how the 2 SVF files (4-pin vs 6-pin) are to be used differently. 2. The SVF files are HUGE. I noticed that the programming is done in 11-bit chunks. Is there a way to create a smaller SVF file, a binary SVF file? I am trying to fit it into the system controller's FLASH. Thank you, Andre