TDE1767DP Output logic and Reset pin functionality
We have selected TDE1767DP TDE1747FPT part as a replacement part for TDE1767DP. I have two questions in this case.
The first question is: Both the parts has a capability to shut down the driver when internal dissipation becomes too high to prevent excessive heating. But in addition to this, TDE1767DP part has Reset Pin (Pin No: 5) which controls the output as below:
The output stays null after the overheating is off, if the reset input is low.
If high the output will alternatively switch-on and off until the overload is removed.
I would like to know how this (Reset) functionality is controlled when the overheating is in off state in TDE1747FPT.
Second Question: It is regarding the output logic. To get the similar output when we use TDE1747FPT IC in place of TDE1767DP do we need to swap the inverting and non inverting inputs because the output side of TDE1747FPT has the NPN transistor logic and TDE1767DP has the PNP logic.