The idea of creating debug microcontrollers, in which the pins would have set-diodes that would display the process of data exchange.
I had an idea for debug microcontrollers, so that there were microcontrollers with a light display of the receive-transmit channel. Such chips will be in the category of debug chips, when a circuit is being developed and it is much easier for the code to. When there are many microcontrollers in operation on a single-wire protocol and each with its own external functions, then heaps of wires and external LED displays become inconvenient. And everything is so compact and clear.
And this is an example of the rgb version of displaying data exchange processes.