"The interface firmware FAILED to reset/halt the target MCU" .txt with STEVAL-SPIN3202
Hello,
I am working with STEVAL-SPIN3202 to develop motor control solution. I am using the Motor Control Workbench 6.2.1.
I could generate the project using the workbench, however when i Connect the evaluation board, window with FAIL.txt opens which reads "The interface firmware FAILED to reset/halt the target MCU".
Thus I am not able to connect to the board. I have tried connecting to the board using ST-Link Utility, however it gives the error message "Can not connect to target".
I have tried some of the solution mentioned on the forum but the issue still persist.
Please guide me so that i can get my motor running.